{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a SoMove configuration file be loaded to the Altivar drive while it is running the motor?
Issue:
Can the program be backed up from the drive using SoMove while the drive is running?

Product Line:
All drives and soft starts

Environment:
All

Cause:
None

Resolution:
No, you cannot download from SoMove to the drive while it is running the motor.  This is the same as standard programming.  Most parameters cannot be changed while the drive is running. You will have to stop the drive before transferring the file.

You can connect and load from the drive to SoMove while it's running.

Schneider Electric Saudi Arabia