Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do we have any instructions on how to set up the STO, SS1 and SLS safety inputs on the ATV32 drives?
Issue:
Instructions on how to set up STO, SS1 and SLS safety inputs on the ATV32.

Environment:
Altivar ATV32

Cause:
All

Resolution:
There are three safe inputs that can programmed on the ATV32 drives.
STO= means Safe Torque Off
SS1= means Safe Stop 1
SLS= means Safely-limited speed

These inputs can only be assigned or programmed using SoMove software
Basic instructions Open SoMove software
You will need to connect the drive before you assign any of the safety inputs.
Choose the Safety function TAB
Choose configure
Type in your password or 6969 enter
Choose one of two inputs SLS or SS1 and assign them to a logic input or assign STO.

See the attached files for assistance.

Program application and programming assistance see the S1A45606 safety manual

Schneider Electric Saudi Arabia

Attachment(s)
S1A45606.pdf [2.51 MB]
ATV32 safety function logic input assignments.pdf [200.46 KB]