Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you get a pulse output on a variable speed drive?
Issue:
Can you get a pulse output on a variable speed drive?

Product Line:
Altivar Machines, Altivar 340

Environment:
All models and serial number

Cause:
Pulse output needed for signal sent back to PLC

Resolutuon:
The  ATV340 product has a PTO (Pulse Train Output) available on connector CN4.
It is a  5Vdc differential RS422 signal with the output frequency greater than or equal to 500 kHz.