Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you update the Multi-Loader's firmware?

Article available in these languages: Spanish

Issue:
Multi-Loader's firmware update

Product Line:
Multi-Loader programmer

Environment:
All

Cause:
Needs to update the Multi-Loader's firmware.

Resolution:
There are two methods for updating the Multi-Loader:
• The user connects the Multi-Loader to the PC (with the SD card in the Multi-Loader) and transfer the file for updated application device to the card SD. The Multi-Loader is then updated as soon as it is turned on.
Or
• The user copies the update file to the SD card, (with the SD card in the PC) then inserts the SD card into the Multi-Loader; the Multi-Loader is then updated as soon as it turned on.
These instructions are included in the Multi-Loader Simplified Manual:

Please note the firmware version you currently have in determining which update file you need. For example, there is one file to update the firmware from V1.10 to V3.14 and one file to update the firmware from V3.08 to V3.14.

Schneider Electric Saudi Arabia

Attachment(s)
Multi-loader_MLD_FW_from_V3.08_to_V3.18.zip [127.01 KB]
MLD FW from V3.08 or higher to V3.14.7z [109.34 KB]
MLD FW from V1.10 to V3.14.7z [109.4 KB]
Multiloader User Manual.pdf [2.58 MB]
Update MLD.doc [63 KB]
Schneider-Multi-Loader-Simplified-Manual.pdf [5.72 MB]