Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can M241 control LXM28 via modbus ?
In fact ,LXM28 can not be control with Modbus ,CN3 only can be used as commissioning interface for SoMove .
Modbus (commissioning interface) 1
Modbus (commissioning interface) 2Modbus (commissioning interface) 3Modbus (commissioning interface) 4

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: