Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Use the serial port 1 of Twido as Modbus port,could the program cable be used as the communication cable?
No,the communication cable connecting to serial port 1 should short pin 5 and pin 7.