Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between Ref 1B switching and Ref 2 switching on the ATV61 and ATV71 drives?

Article available in these languages: Spanish

Issue:
Difference between Ref 1B switching and Ref 2 switching on the ATV61/71 drives.

Product Line:
Altivar ATV61 and ATV71 drives

Environment:
All

Cause:
Customer needs to know why do we have two reference switching on the ATV61 and ATV71 drives?

Resolution:
Ref 1 B switching will allow you to switch between Ref 1 channel in Menu 1.6 and Ref 1 B channel in Menu 1.7.
Ref 2 switching will allow you to switch between Ref 1 channel in menu 1.6 and Ref 2 channel in menu 1.6

See the attached programming manual for programming assistance on setting them up.

Schneider Electric Saudi Arabia

Attachment(s)
atv61_programming_manual_en_1760649_08.pdf [4.35 MB]