Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
why can't I connect to the CPU using Unity Pro or Control expert ?
A BMXXBE module (rack extension module) may be installed, without an extension rack connected.
remove the xbe module from the local rack, or add an extension rack.