Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I verify that the analog output of the ATV61 or ATV71 drive is correct?
Issue:
Trying to verify that the analog output of the ATV61 or ATV71 drive is correct.

Product Line:
ATV61, ATV71

Environment:
All models and serial numbers

Cause:
None

Resolution:
1.  Set the Maximum Frequency parameter (tFr) to 60.
2.  Set the "AO1 type" to current and "AO1 min output" to 4.
3.  If a wire is connected to AO1 then remove it..
4.  Connect your mA current meter in series between AO1 and COM.
5.  The value should approximate the "AO1 min output" from step 2.
Note: The analog output can also be seen by looking at the "Analog Outputs Image" in the monitoring menu under logic input map.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre