Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many Remote IO drops does an M580 PLC support?

Article available in these languages: Spanish

M580 CPU                      |        Max Remote I/O Drops
--------------------------------------------------------------------------------

BME P58 2040                |              8
BME P58 3040                |              16
BME P(H)58 4040           |              16
BME P(H)58 5040           |              31
BME P(H)58 6040           |              31
--------------------------------------------------------------------------------
A "Rack" is defined as a backplane which holds devices.
A "Drop" is defined as the rack which are connected to CPU as a node on the RIO network.
A Drop can contain multiple racks by use of the BMXXBE Rack Extenders.