Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What can cause an INF1 (Rating Error) on an ATV61 or ATV71 drive?
Issue:
Causes for INF1 (Rating Error) on an ATV61 or ATV71

Product Line:
ATV61/ATV71 drives

Environment:
INF1 faults

Cause:
n/a

Resolution:
Check the part number of the power board. Check the graphic terminal the size and the voltage of product. Check the power identification number.