Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the MTBF on the BMXNOC0401?

Issue:
What is the MTBF on the BMXNOC0401?

Product Line:
BMXNOC0401

Resolution:
The MTBF at various conditions (in hours) is presented below in this table:

ProductMTBF 30° ContinuousMTBF 30° IntermittentMTBF 60° ContinuousMTBF 60° IntermittentMTBF 85° ContinuousMTBF 85° IntermittentNb Cpt MissingNb Cpt Missing * QtyNb Cpt Total * QtyRatio Nb Cpt Missing / Nb Cpt Total
BMXNOC04011554139.217896891.553908288.313624804.358548512.653425723.762183902.10%

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)