Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the ribbon cable on the ATS48 control board available as a separate item?
Issue:
Is the ribbon cable on the ATS48 control board available as a separate item?

Product Line:
Altistart 48 ATS48

Environment:
All models

Cause:
The ribbon cable is needed to repair the ATS48.

Resolution:
The ribbon cable that connects the control board to the power board is not offered as a separate item. It is included with the VX4G481 control board only.