Issue
Web Designer help mentions that 1000 variables can be use in a projects, however this doesn’t apply when the RecipeDb service is used with an automatic request.
Product Line
Factory cast HMI (WMY, NMW)
Resolution
When using an automatic request with the recipeDB, the maximum number of variables (integers) should be limited to 300 to insure the stability of the Tsxwmy100.
Web Designer help mentions that 1000 variables can be use in a projects, however this doesn’t apply when the RecipeDb service is used with an automatic request.
Product Line
Factory cast HMI (WMY, NMW)
Resolution
When using an automatic request with the recipeDB, the maximum number of variables (integers) should be limited to 300 to insure the stability of the Tsxwmy100.
Released for:Schneider Electric Saudi Arabia