How can we help you today?

Does a MIB database file available for a module BMX P58 4020?

Actualy a private MIB is not implemented in M580.
If IO scanning communication table is needed, then Modbus TCP (function code 8/21) can be used.
The other Standalone M580 CPU are in the same situation (BMXP58X040, BMXP58X020, BMXP5820X0, BMXP5840X0).

Schneider Electric Saudi Arabia