Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the meanings of the various status LED operations on an Enercept Meter?
Issue
A user would like to know the various reasons behind the status LED's on an Enercept Meter.

Product Line
Enercept Meters

Environment
Enercept meter troubleshooting

Cause
The Enercept meter has a status LED for diagnostic purposes. A user would like to know more information about the various states of the status LED for troubleshooting.

Resolution
If the LED blinks greenThe product is functioning normally. It blinks slow, approximately one second on, then one second off.
If the LED is red and blinking slowlyIn most cases, incorrect wiring will cause the STATUS LED to blink RED (slowly). However, a power factor lower than 0.5 could cause the LED to blink this way, even if the unit is installed properly.
If the LED is red and blinking quicklyCT’s maximum current rating has been exceeded
If the LED does not blinkCheck fuses and voltage connections. STATUS LED should blink regardless of CTs, Modbus connections, and DIP switch settings.
If the LED does not blink.When the unit is wired on the load side of an adjustable frequency drive and the LED does not blink, the unit’s thermal fuse could be blown. The unit must not be installed on the load side of an adjustable frequency drive.