Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I use the embedded Ethernet port on the M221 as a Modbus TCP/IP client?

Article available in these languages: Spanish

Issue:
Using the embedded Ethernet port on the M221 as a Modbus TCP/IP client


Product Line:
TM221, Machine Expert Basic


Resolution:
Yes. The embedded ethernet port on the M221 is capable of Modbus TCP/IP communication as a server or client. For Modbus TCP/IP server function you can use either the EXCH3 or the READ_VAR / WRITE_VAR function blocks to read/write to and from the server device.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)