Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What will cause the ATV212 not to go into local mode when pressing the LOC/REM button?

Article available in these languages: Spanish, Korean


Issue:
What will cause the ATV212 not to go into local mode when pressing the LOC/REM button?

Product Line:
ALTIVAR 212, ALTIVAR 21

Environment:
All serial number

Cause:
When pressing the LOC/REM button the drive will not go to LOC mode.

Resolution:
This could possibly be due to parameter F732 (LOC/REM button disabled) being set to 1. If so, set F732 to 0.   However, if the LOC/REM button is not disabled, then it is likely, the keypad is defective, the drive will need to be replaced.