Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the code FLU on the display of the Altivar Drives?
Issue:
FLU on the display of a drive.

Product Line:
Altivar 61
Altivar 71
Altivar 320
Altivar 340
Altivar 930

Environment:
All models

Cause:
N/A

Resolution:
FLU is a VFD state/status.
It is not an error code.
FLU indicates that motor fluxing is in progress.  Review the Programming manual for your drive to identify how to enable or disable Fluxing.