Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the recommended Fiber Optic specs for the ConneXium TCSESM063F2CU1 switch?

Article available in these languages: Spanish

Fiber media type. Multi Mode
Wavelength. 1300nm
Fiber. 50/125μm
System attenuation. 0-8 dB
Expansion. 0-5 km
Fiber Data. 1.0 dB/km, 800 MHz km