Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why CT Reference numbers mentioned in drawing and catalog of the BlokSeT are not same?
The CT reference numbers are changed to new nomenclature as per the Schneider rules. The old reference numbers are 5 digit number. This reference number does not give details like, Type of Form (Cable or Bus bars) or the primary or secondary rating of the CT.

New nomenclature of CT gives the details like primary and secondary rating of the CT, type of form like cable or bus bar profile.


To Co-relate the old CT reference number with new CT reference number, please refer to the attached file.

Schneider Electric Saudi Arabia

Attachment(s)
CT Reference.xlsx [12.57 KB]