How can we help you today?

PlantStruxure PES [V4.0]: Ports used by PES / Unity / VijeoCitect

The following ports must be unblocked for certain functionality to work either in PES or on a standalone installation of Unity or VijeoCitect. If these ports are blocked by the firewall you may experience problems such as establishing communications when running VijeoCitect Runtime in Multi-process mode (separated Client, I/O Server processes).

This knowledge base article is applicable for only PES4.0.

VijeoCitect V7.40SP1 Port
I/O Server2082
Report Server2084
Alarm Server2080
Trend Server2085
Alarm Database Port5482
PES V4.0
System Server9950
Unity Pro Simulator502











Schneider Electric Saudi Arabia