Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will the PM5000 series meter change the energy units on the display after exceeding 1000 GWh?
Issue
The PM5000 series meter has accumulated over 1000 GWh of energy, user wants to know if the display with change units to TWh automatically.

Product
PM5000 series meter

Environment
PM5000 with high energy use

Cause
The units for energy consumption is automatically adjusted as energy is consumed

Resolution
The PM5000 meter will automatically change from GWh to TWh.