Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What fuse size is needed for the ATS22 CL1 CL2 control circuit?

Issue:
Looking for the fuse size needed for CL1-CL2 on ATS22 soft starts

Product line:
ATS22, Altistart 22


Resolution:
The CL1 - CL2 control voltage input should have a 1A fast acting fuse, or 1A circuit breaker for each ATS22 unit.  This applies to the 120V and 230V control supplies (Q, S6 and S6U).

See attachment

Schneider Electric Saudi Arabia

Attachment(s)
ATS22 fuses.png [133.36 KB]