Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will the ATV61 or ATV71 drives 4 to 20 ma input speed signal control the drive motor speed between LSP to HSP or 0 to 60hz?
Issue:
ATV61 or ATV71uses 4-20mA input speed signal to control the motor speed between LSP to HSP.

Product Line:
Altivar ATV61

Environment:
All

Cause:
They have low speed LSP set to 45 hz but they want the drives analog input to allow the drive to run between 0 to 60hz not low speed to high speed.

Resolution:
The Drive wills analog inputs will allow the drive to run between Low speed to high speed.   If you want to have a low speed setting above 0 and still want the drive to follow 0 to 60hz then set the Reference Template Parameter (BSP)  in Menu 1.5  to Pedestal mode.

Menu 1.5 programming below.


pedestal