Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What can cause an PTFL fault on the ATV61 and ATV71 drives?
Issue:
PTFL fault on the ATV61 and ATV71 drives.

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Drive is faulting on power up.

Resolution:
This is a PTC error fault.   Check to see if the PTC switch is turned ON if so check to see if the PTC input is open or shorted.