Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can you find the Amp ratings for ATV212 drives?

Issue:
Amp ratings for ATV212 drives.

Product Line:
ATV212, Altivar 212

Environment:
All serial numbers for ATV212 Drives

Cause:
N/A

Resolution:
The drive output ratings are available in the Installation manual.
ATV212 Installation manual is attached.

Schneider Electric Saudi Arabia

Attachment(s)
ATV212_Installation_manual_EN_S1A53832_04.pdf [6.09 MB]