Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the BCPME Natively Supported in PME?

Issue:
Is the BCPME Natively Supported in Power Monitoring Expert?

Product Line:
Power Monitoring Expert 7.2.2
Power Monitoring Expert 8.x

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Environment:
Configuring the BCPME meter in Power Monitoring Expert software

Cause:
The user wants to know how to configure the BCPME in PME software

Resolution:
PME does not have a specific driver for BCPME. Therefore, the user will have to use the BCPM driver for BCPME.

  1. Add the site using the BCPME IP address.
  2. Create a device underneath that site as a "serial device on an Ethernet gateway" using the BCPM device type
  3. Enter unit ID 100 for Modbus TCP.

(NOTE: The BCPME is the same as the normal BCPM A, B, and C types with the exception that an ethernet gateway is embedded into the physical device and onboard logging (a 1-deep data recorder))