Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the wiring diagram for the HMISCU Analog Inputs and Outputs?
Issue
Where can I find the wiring diagram for the Analog Inputs and Outputs on the HMISCU?

Product Line
Harmony HMISCU (Analog Models: HMISBC, HMISCU6B5, HMISCU8B5)

Environment
Physical HMI / PLC

Resolution
The diagram below shows the wiring diagram for the Analog Inputs and Output on the HMISCU:

Wiring Diagram

For more information about the HMISCU, please see the Harmony SCU HMI Controller, Hardware Guide (pdf link)
Web Link: Harmony SCU Controller - Hardware Guide