Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I add a switch to access the System Configuration screen on an HMI with Vijeo Designer V6.2?
Issue
How can I add a switch to access the System Configuration screen on an HMI with Vijeo Designer V6.2?

Product Line
Vijeo Designer

Environment
HMI Configuration Software

Resolution
Steps:
1) Go to the Switch Setttings by doubleclicking on the Switch you wish to Edit on a Panel.
2) Change the Operation to System.
3) Select Configuration.
Switch Settings dialog

After downloading this project to a physical HMI, pressing this button will bring an operator to the System Configuration screen.