Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can VISTA display avi?
Avi files do work in Vista with a limitation (and are supported in Grouping Objects in PME 7.2 WebReach with IE) which is Vista can only display AVI clips originating from either an uncompressed AVI file or from an AVI file that was compressed using run-length (BI_RLE8) encoding. Also the AVI file must not have a sound channel.