Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the TM221 have the capability to do 120vac Inputs and Outputs?
All the TM221's that end with the letter "R" are Relay Outputs and can do 120vac Outputs.
To do 120vac Inputs add a TM3DI8A module to the TM221.