Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will SoMove display the VW3A3408 resolver option cards serial number, part number or firmware version?
Issue:
Is SoMove showing option card serial number, part number or firmware version?

Product Line:
Altivar 71 only with the VW3A3408 resolver option card

Environment:
All

Cause:
Wants to know if SoMove will display the serial number, part number and firmware number.

Resolution:
SoMove will only display the reference part number of the card only see example below.

nh