Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I find information on dynamic braking resistors to use with the ATV32, ATV312 and ATV71 drives only?
Issue:
Dynamic braking resistors to use with the Altivar drives.

Product Line:
ATV32, ATV312 and ATV71 Drives

Environment:
All

Cause:
Needs to know if the drives come with a DB resistor?

Resolution:
The braking resistor is not included on the ATV32, ATV312 and ATV71 Drives, and if needed must be purchased separately.
In the US, we have partnered with a resistor company named Powerohm to provide a full range of options.
See attached document for information on sizing and selecting DB resistors from Powerohm.
Note that any technical questions related to the resistors themselves should be directed to Powerohm and the document includes their contact information.

Schneider Electric Saudi Arabia

Attachment(s)
POWEROHM_SELECTION AND PRICE GUIDE_Y13M03D15.xlsx [1.38 MB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: