Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you set the line termination resistor on the ATV212 drive set up for Bacnet protocol?
Issue:
Line termination resistor on the ATV212 drive set up for Bacnet protocol.

Product Line:
Altivar ATV212

Environment:
All

Cause:
Needs to terminate his Bacnet line and wants to know how to set the drive up.

Resolution:
Switch SW103 is the line termination resistance switch to put 120 ohms across the data pins A and B.