Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there an Altivar Drive available that can convert 220V single phase input to 460V three phase output?
Issue:
Altivar Drive option capable of converting 220V single phase input to 460V three phase output

Product Line:
All Altivar Variable Frequency Drives and Altistart Soft Starters.

Environment:
All models, All serial numbers.

Cause:
Customer has 460V three phase motors available but only 220V single phase power available.

Resolution:
No, there are no drive products that can convert 220V single phase power to 460V three phase power. There are drives in our product lineup that can convert single phase 230V to three phase 230V. If the motor is dual rated for 208-230V / 460V operation, then wiring it for 230V may be a better option.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: