Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
BMXFTW308S cable diameter
Issue
This Resolution explains the maximum diameter for the BMXFTW308S cable.


Product Line
BMXFTW308S


Resolution
The cable diameter is 11.2mm.

The BMXFTW308S cable is a shielded cable used with  the M340 I/O modules.
It has a 28 pin terminal block on one end and color-coded flying leads on the other end.image1