Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
I have PLC type TSX3721101 and it has the lamp I/O IS red , while RUN lamp is green & TER lamp is orange, what is the problem?
It seems from the error that PLC is in RUN mode and its communicating. There seems to be an issue with IO's etc.
IO LED (red) is lit to show a fault relating to the inputs/outputs: supply fault or at least one channel tripped, module missing, not configured or out of service. So kindly go online with PL7 software and troubleshoot and check for any errors on modules.
Suggestion is to troubleshoot, identify the faulty modules or else if any and replace or correct the same. The I/O error must go.