Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does the fault code LFF2 fault mean on the Altivar drives?
Issue:
LFF2 fault code on the ATV61 or ATV71 drives

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
The drive is powering up with a LFF2 fault.

Resolution:
LFF2 LFF3 and LFF4 are all 4 to 20mA loss of follower faults.
Check your programming in the 1.8 Fault Management menu under 4 to 20mA Loss.  Turn this function off if you are not using it.
Check your analog signal to see if the drive is getting a 4mA min signal.