Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Changes between Unity 7 and Unity 8 for READ_VAR and WRITE_VAR
Issue
Changes between Unity 7 and Unity 8  for READ_VAR and WRITE_VAR

Product Line
Unity 7, Unity 8

Environment
Windows 7, Windows 8

Resolution
The 'types Library Manager shows that the version has changed in the READ_VAR and WRITE_VAR blocks.  The
online help and release notes do not describe the changes between Unity 7 and Unity 8  for the READ_VAR and
WRITE_VAR.



The changes is described below.

'READ_VAR':
Unity 7.0 READ_VAR version V1.00

Unity V8.0 READ_VAR version V1.01
  • Added support Ethernet Remote IO drops.

'WRITE_VAR':
Unity 7.0 WRITE_VAR version 1.01

Unity 8.0 WRITE_VAR version 1.02
  • Added support Ethernet Remote IO drops.