Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can Unity Pro PLC system words and bits be accessed within an LL984 ladder logic section?
Issue:
Trying to view system words in an LL984 section in Unity Pro.

Product Line:
Unity Pro programming software

Resolution:
No, the user would have to create an IEC section in order to view PLC system words or bits in Unity Pro.
They can be accessed through an Animation table.