Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Incorrect OS Loader description when updating a 140NOC78X00 DIO Head module
Issue
This document addresses an issue when updating the firmware in a Quantum 140NOC78X00 DIO Head module.

Product Line
Quantum

Environment
OSLoader

Resolution
When loading firmware into a Quantum 140NOC78X00 DIO Head module, the OS loader screen for the firmware about to be loaded indicates that this firmware is for a 140CRP31200/140NOC78X00 Head as seen in the attached screenshot.  The reference to the 140CRP31200 is incorrect.  The firmware is only loadable into a 140NOC78X00 DIO Head module and is not intended to be loaded into a 140CRP31200 module.

Additional Information
See attached screenshot of the OS Loader.

Schneider Electric Saudi Arabia

Attachment(s)
BadOSLoaderDescription.jpg [51.94 KB]