Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to determine the logic input assignments on an ATV61/71 drive?
Issue:
Logic input assignments on an ATV61/71 drives

Product Line:
ATV61/71

Environment:
All products of ATV61/71

Cause:
N/A

Resolution:
Logic input assignments can be viewed by going into the IO map
Drive Menu ~> 1.2 Monitoring Menu ~> IO Map ~> Logic Input Map
Move the cursor over to desire logic input and hit enter to view its assignment.
This same Logic Input map shows the current state of the logic input.