Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the changes on the Micrologic trip unit performance when we install a LT Off Rating Plug?
When you use the LR off plug that means Ir = 1 and Tr = very far from standard times delay (near infinity). There is a direct relationship between load shedding and the long time delay protection so for this reason the load shedding will remain off too. You can replace it with the 3 alarms called Ia max, Ib max and Ic max, each alarm have to work in relationship with 3 contacts of the M6C. The power shedding feature is not affected if you install a LT Off Rating Plug