{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the ATV212 be used on a positive displacement pump?
Issue:
Is ATV212 designed for or a constant torque application such as Positive Displacement Pump?

Product Line:
Altivar 212, S-Flex

Environment:
All models and serial numbers

Cause:
N/A

Resolution:
The ATV212 is designed for variable torque applications. A positive displacement pump is considered a constant torque application so the ATV212 is not recommended.

Schneider Electric Saudi Arabia