{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the maximum roof load rating for NetShelter SX and SV cabinets?
Issue:
Information regarding the maximum load rating for the roof is required

Product Line:
NetShelter SX, NetShelter SV

Environment:
All versions and serial ranges.

Cause:
The load rating should not be exceeded.

Resolution:
The roofs of both the NetShelter SX and SV cabinets are rated to 200 lbs.

Schneider Electric Saudi Arabia

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: