Search FAQs
Where are the S-Flex factory settings listed?
Issue:
S-Flex factory settings listed request
Product Line:
S-Flex
Environment:
All models
Cause:
None
Resolution:
The factory settings for the S-Flex Adjustable Speed Enclosed drive (Class 8839) can be found in Table 18 of the instruction bulletin 30072-451-83 (see below).
https://www.se.com/us/en/download/document/30072-451-83/
Also, the factory settings of the S-flex are stored in a reserved memory location within the drive by the factory during production. To return the S-flex drive to the default programming, press MODE until AUF is displayed, then scroll down to parameter TYP. Press ENTER, then up until 8 is displayed on the right hand side of the screen. Press Enter to reboot the drive and return to the factory default programming for the S-flex system.
IF you are installing a new ATV212 drive in an existing S-Flex enclosure, the parameters will NOT be stored in the drive so you must follow the programming changes listed below.
S-Flex factory settings listed request
Product Line:
S-Flex
Environment:
All models
Cause:
None
Resolution:
The factory settings for the S-Flex Adjustable Speed Enclosed drive (Class 8839) can be found in Table 18 of the instruction bulletin 30072-451-83 (see below).
https://www.se.com/us/en/download/document/30072-451-83/
Also, the factory settings of the S-flex are stored in a reserved memory location within the drive by the factory during production. To return the S-flex drive to the default programming, press MODE until AUF is displayed, then scroll down to parameter TYP. Press ENTER, then up until 8 is displayed on the right hand side of the screen. Press Enter to reboot the drive and return to the factory default programming for the S-flex system.
IF you are installing a new ATV212 drive in an existing S-Flex enclosure, the parameters will NOT be stored in the drive so you must follow the programming changes listed below.
Released for:Schneider Electric Saudi Arabia
Explore more
Explore more