{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can SoMove V2.2 be used with Windows 8
Issue:
Wanting to know if he could use SoMove V2.2, with Windows 8?

Product Line:
ATV32 , ATV61, ATV312, ATV212, ATV71, ATV12

Environment:
All

Cause:
Installation / Setup

Resolution:
Yes SoMove v2.2 is compatible with Windows 8 (and 8.1).

SoMove V2.2 has been obsoleted...current version (as of April 2017) is V2.6

Schneider Electric Saudi Arabia