Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement for the PCMCIA memory card XBTMEM08 and XBTMEM16?
Issue
What is the replacement for the PCMCIA memory card XBTMEM08 and XBTMEM16?

Product Line
Telemecanique HMI - XBTF HMI family

Resolution
The XBTMEM08 and XBTMEM16 were the memory cards (8mb and 16mg) for the Legacy Magelis XBTF (circa 2003).  This Magelis XBTF HMI and the associated memory cards are no longer available.

The XBTMEM08 and XBTMEM16 memory cards have been replaced with the following:
XBTZGADT (PCMCIA to CF card adapter)
XBTZGM128 (128mg memory card)

Note: The Magelis XBTF HMI should be updraded to an HMIGTO.