Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to connect an HMIGTO to a Micrologix 1400 PLC?
Issue:
How to connect an HMIGTO to a Micrologix 1400 PLC?

Product Line:
Magelis HMIGTO

Resolution:
The cable combination to use is: Dsub9 [PLC side] <-- XBTZ9730 + XBTZG999 + D25 to D9 Converter (generic) --> Dsub9 [HMI Side]

You can also use XBTZ9730 + XBTZG919